Responding to the need for high-speed imaging with improved visible and near infrared (NIR) sensitivity, Baumer has engineered two outstanding GigE cameras: the TXG02, a VGA camera capable of 100 fps, and the TXG12, a 1296 x 966 pixel camera capable of 30 fps. These new TXG cameras achieve their impressive visible and NIR spectral response by incorporating CCDs with sensitivity-enhancing ExView technology. Baumer’s camera innovation includes convenient features such as an adjustable “Trigger Delay”, a new “Timer” function and a “Sequencer” which captures multiple images while varying the exposure times. This powerful combination of high performance imaging, advanced features and a Baumer-GAPI generic programming interface, helps users quickly adapt the cameras for the best solution to a particular imaging application.








![[Translate to int-en:] 399](http://www.baumer.com/typo3temp/pics/2901-1-DCH_add0405cf4.jpg)