CombiLyz: Conductivity and temperature at a glance

quinta, 5. junho 2014

CombiLyz by Baumer was developed for precise analysis and differentiation of media in the food and pharmaceutical industries and in water treatment technology.

Baumer is expanding its CombiSeries to include a new conductivity sensor. CombiLyz is the name of the newest sensor, which was developed primarily for precise analysis and differentiation of media in the food and pharmaceutical industries and in water treatment technology. The CombiLyz sensor features the compact CombiSeries housing. With its IP 69 K protection class and entirely stainless steel design, the hygienic version can withstand even the toughest conditions.

In practice, the CombiLyz is ideally suited for use in CIP and SIP processes, for monitoring concentrations in liquids, or for phase separation of different media. A selection of 14 measuring ranges from 500 µS/cm to 1000 mS/cm is available. The sensor's measurement results are highly accurate, with a maximum deviation of <1 %. It also boasts an impressively fast response time of less than 0.3 seconds for conductivity measurements and less than 15 seconds for temperature measurements.

The standard version includes the proven CombiView display, which can display multiple process variables at the same time. This includes the concentration, temperature, current output, switching states and device status in addition to conductivity. The large display also means that users can read the measured values even from greater distances. Furthermore, the background color of the display works like a traffic light system (red/green), depending on whether the measurement results have reached a critical value that requires user intervention. Settings can be changed easily using the touchscreen display even while the process is running.

More information: www.baumer.com/combilyz/

facebooktwitterlinkedin