Fácil integração, flexibilidade e inteligência – Sensores NextGen com IO Link

segunda, 27. julho 2015

Through the integration of the communication interface IO-Link for the sensor principles diffuse mode sensor with background suppression and SmartReflect (the light barrier without a reflector), the optical O300 and O500 NextGen sensors have improved their already outstanding efficiency. The IO-Link interface facilitates the rapid startup of systems through the automated transmission of various parameters such as sensing distance accurate to the millimeter, light or dark operate, or switching points. In addition, the new Baumer filter functions guarantee the safe and reliable detection of difficult objects, for example objects with holes.  Through the option of automatically changing the locking times of the sensors, these sensors also have a high level of user-specific functional reliability.

facebooktwitterlinkedin