Web interface made even better – VeriSens Software 2.4 with new functionalities

Wednesday, 9. April 2014

The VeriSens human-machine interface is now even more clearly structured and provides the user with supporting information.

Since the first quarter of 2014, the Baumer VeriSens vision sensors have come with latest 2.4 software of the VeriSens Application Suite.

This first configurable web interface for vision sensors by Baumer is setting a milestone in simplified creation of human-machine interfaces. Software update 2.4 provides an even further enhanced user interface for more convenient touch operation. Enlarged buttons and short info texts on the related feature checks support the user who often is confronted with small-sized operating panels. Now, the OEM can even configure the VeriSens web interface to match the customer’s corporate identity specifications such as corporate colors and logos.

Easy to operate, the web interface will be configured within a few minutes and in parallel will enhance performance also in conjunction with still commonly used old generation browsers. Now, there is also more to some selected feature checks. The new, high-performance pattern comparison is intuitive to operate and opens up new application potential in packaging control. Enhanced backup and restore functionalities allow utilizing the FTP server not only for defect images but also for backup.

A software update will upgrade all VeriSens models of the XF, XC ID and CS series which are already used in the field with the new feature package.

facebooktwitterlinkedin