Series 66 fibre optic sensors – New fiber optic sensors – enhanced ease of use

Monday, 15. November 2010

With the new Series 66 fiber optic sensors Baumer enhances the ease of use in fiber optic applications.

[Translate to int-en:] 496

  • User-friendly interface
  • Version with reduced cabling effort
  • Convenient teach-in functionality with auto-tuning
  • Extreme long-term stability

Amongst others this is achieved with a user-friendly, clearly arrangedinterface and an easy teach-in process.

Sensitivity and sensing distance can easily be adjusted using three different sensing modes. Within these modes the sensitivity is optimized automatically. The learning of the threshold via auto-tuning facilitates the teach-in process considerably, because it is not necessary to access a special menu. Manual refinement is possible using the +/- buttons. The nominal range of the sensors is 240 mm at a response time of 250 μs.

With the master/slave version, up to 16 sensors can be connected together to one unit. The simplified wiring concept reduces cabling effort and installation time. The reciprocal influence of several sensors can be suppressed and the Series 66 sensors can be combined with those of Baumer's multifunctional Series 67 without difficulty. Ingenious measures ensure long-term stability and guarantee precise and stable switching states over the entire service life of the sensors.

Together with the comprehensive portfolio of fiber optic heads

facebooktwitterlinkedin