- 1Products
Baumer Group
Description

- 2Industries
- 3Company
Baumer Group
Description

- 4Latest News
Baumer Group
Description

- 5Services
Baumer Group
Description

The following services are available for registered users:
You may register online at any time for free of charge:
Registration member area "Industrial cameras"
To register für the Member Area "VeriSens® vision sensors" please feel free to contact us under www.baumer.com/worldwide
"On the occasion of the "Supplier Days 2011" ABB AB, Process Automation, Sweden gives the award for "Best Innovation 2010 " to the Baumer Competence...
Double-sided mounting for high loadsDual protected electronicsInsulated steel shaft for protection against shaft currentsHigh performance line driver...
The new CFDK 25 capacitive sensor in ultra flat housing has a variety of mounting options. The special mounting frame facilitates low-cost assembly...
With the VeriSens® ID-110 Baumer offers a vision sensor enabling faulty imprints e.g. of best-before dates to be reliably detected and discharged in...
The latest generation of VeriSens® vision sensors from Baumer sets new standards of operating simplicity and dependability.
[Translate to int-en:] Baumer's industrial pressure gauge MEX5 is specially designed for use in corrosive atmospheres and fluids.
The new CMOS cameras (HXC20 and HXC40) with Global Shutter are designed for high speed applications and come equipped with many useful functions such...
The resolution of the IPRM 12 inductive sensor has been significantly improved. The sensor now measures with a resoution of up to 4 nm, which is to...
Baumer's PBSN general purpose pressure transmitter series can now be used in media temperatures up to 150°C. This is made possible by means of a...
For the fourth time in a row Baumer Switzerland received the award TOP Employer. The neutral judgment of the Corporate Research Foundation (CRF)...