Archive

[Translate to int-en:] 424
Monday, 17. January 2011

New laser sensor for particularly demanding applications

With three news sensors Baumer expands its OADM 13 family of distance measuring laser sensors. Thanks to innovative technical improvements, the laser...

facebooktwitterlinkedin
[Translate to int-en:] 436
Wednesday, 8. December 2010

Baumer DSRC Strain Rings Are Overload-safe and Save Time

With the strain ring series DSRC, Baumer offers flexible solutions for measuring cyclical processes such as tension, compression, and torque. The...

facebooktwitterlinkedin
[Translate to int-en:] 411
Monday, 6. December 2010

Encoders, cable-pulls and inclination sensors

Hardly any other application demands more from a sensor product than outdoor deployment. Operation and functionalities must not be affected by...

facebooktwitterlinkedin
[Translate to int-en:] 420
Monday, 29. November 2010

PBMN pressure transmitter uses piezo-resistive and thin-film...

Baumer’s industrial pressure transmitter PBMN achieves maximum precision in measuring both low and high pressures by using different sensors. For...

facebooktwitterlinkedin
[Translate to int-en:] 414
Monday, 22. November 2010

Distance measuring sensors – high performance in miniature format

As a pioneer in terms of miniaturization Baumer offers the smallest, and at the same time most powerful sensors in its measuring sensors‘ portfolio....

facebooktwitterlinkedin
[Translate to int-en:] 404
Monday, 15. November 2010

Large selection of robust stainless steel encoders

Sensor products deployed in harsh environments demand specific housing and sealing techniques as protection against the prevailing adverse...

facebooktwitterlinkedin
[Translate to int-en:] 401
Monday, 15. November 2010

Encoders with modular Ethernet interfaces

Thanks to high-grade performance merged with ease-of-use, Ethernet provides the ideal basis for effective data communication in industrial...

facebooktwitterlinkedin
[Translate to int-en:] 408
Friday, 12. November 2010

New fiber optic sensors - enhanced ease of use

With the new Series 66 fiber optic sensors Baumer enhances the ease of use in fiber optic applications. Amongst others this is achieved with a...

facebooktwitterlinkedin
[Translate to int-en:] 399
Friday, 5. November 2010

Baumer Expands its Successful GigE Camera Family by 2 New Models

Responding to the need for high-speed imaging with improved visible and near infrared (NIR) sensitivity, Baumer has engineered two outstanding GigE...

facebooktwitterlinkedin
[Translate to int-en:] 395
Wednesday, 3. November 2010

Dual GigE Technology Doubles Standard GigE Bandwidth to 240 MB/s

Baumer’s new SXG cameras combine state-of-the-art Quad Tap sensors from Kodak with innovative Dual GigE technology. This provides the perfect...

facebooktwitterlinkedin