Spindle position system – Target Display with state indicator

Wednesday, 21. July 2010
[Translate to int-en:] 430

  • Target display for manual format aligning
  • One key permanently assigned as target
  • Display: LCD backlit, two lines
  • Interface RS485
  • With or without LED status display

New: A LED state indicator (red/green) that is optionally available enables comfortable visualization of the current alignment status even from remote. The handshake key is saving the edited parameters. Serial interface RS485 enables network of maximum 32 target and spindle position displays with PC or PLC.operating and memory terminals are available."

facebooktwitterlinkedin