Press Release

Safety and flexibility at a glance: CombiView DFON sets new standards in process instrumentation

Baumer is taking functionality, safety and flexibility to a whole new level with its new CombiView DFON display generation. At the ACHEMA 2012 Baumer is unveiling the first two models in this new series, namely the CombiPress PFMx pressure transmitter and the CombiTemp TFRx temperature gauge. Both products feature the new display and thus provide maximum customer benefit. Together with the housing that was also newly developed, the measuring instruments can be configured and implemented according to the individual customer needs, for example, in the food industry or in the oil and gas industry.

The CombiView display is impressive with its presentation of all necessary and desired information at a glance. In terms of the display's visual mode, the user can choose from eight different types: analog, digital or illustration. The large display also means that users can read the measured values even from increased distances. Furthermore, the background color of the display functions as a traffic light system (red/green), depending on whether the measurement results have reached a critical value that requires user intervention. Programming - even during the process - is incredibly simple using the touchscreen display.

The respective housing completes the impressive functions of the new product series. With its protection class IP 69 K and entirely stainless steel design, the hygienic version can withstand even the toughest conditions. In addition, its ability to pivot around two axes facilitates even more installation flexibility.
Reliable and precise measurements are provided by the CombiPress pressure transmitter between -1 and 400 bar and by the CombiTemp temperature gauge between -50 and +400 degrees Celsius.

Baumer's CombiTemp TFRx (li.) and CombiPress PFMx with new CombiView DFON display provide safety and user friendliness in process instrumentation.

Number of letters (including spaces): approx. 1736
This photo is released for publication with this picture.

Press contact

Stefan Diepenbrock
Manager Public Relations
Phone +41 52 728 17 63
Fax +41 52 728 11 44
sdiepenbrock(at)baumer.com
http://www.baumer.com

Baumer Group
20.06.2012
www.baumer.com