Process analysis
We provide the ideal solution for media separation (e.g. beer/water, CIP- dissolutions) or media mixing.
If conductivity in liquids has to be measured like in the food and beverage industry or in the water treatment or enrichment of cleaning agents, the temperature compensated Baumer conductivity sensor guarantees reliable measurement values.
14 switchable conductivity ranges compensated with 7 temperature ranges enables an accurate, qualitative control of the process. In the device both values will be displayed by a protected glass window. Each measured value has an isolated analogue signal output of 4…20 mA available. Four preset measuring ranges can be chosen by an external controller, for example, depending on the recipe specification.
Conductivity transmitter
- Wetted materials: stainless steel, PEEK
- Four configurable measuring ranges (0.5…1000 mS/cm) selectable
- Insensitive to polarization, adhesion and solids
- LC-Display and galvanic isolated current outputs for conductivity and temperature