- 1Products
Baumer Group
Description

- 2Industries
- 3Company
Baumer Group
Description

- 4Latest News
Baumer Group
Description

- 5Services
Baumer Group
Description

There is a trend towards slow speed in motors and generators. Requiring limited gear stages, sometimes even no gearbox at all, these motors save...
There is a trend towards slow speed in motors and generators. Requiring limited gear stages, sometimes even no gearbox at all, these motors save...
Encoders that have to endure hostile ambient conditions must fulfill demanding industry-specific requirements when deployed in mobile transport...
Baumer’s new MTRM 16 hall sensor was specifically developed for the contact-free pulse detection of fast-spinning gear wheels. With its robust metal...
With the level switch LBFS, Baumer offers a cost-efficient and reliable alternative to widely-used vibration level switches. The device is able to...
Baumer’s new CFAK 12 capacitive fill level sensor detects conductive liquids while suppressing dirt particles and detergent residues. When detecting...
For temperature measurement in hygienic applications, Baumer offers the bimetal thermometer TBI with hygienic clamp process connections. It is...
As elsewhere, neither in the incremental encoder field there is an all-in one allround device that is suitable for every purpose. In practice,...
The new member of the SCATEC sensor family was developed in particular to precisely and reliably count newspapers in conveyor belts. The sensor’s...
EtherCAT as an Ethernet solution is conquering all levels of industry automation, from process control level down to field and sensor level. Power...