Press Release

New laser sensor for particularly demanding applications

[Translate to int-en:] 424

With three news sensors Baumer expands its OADM 13 family of distance measuring laser sensors. Thanks to innovative technical improvements, the laser class 1 sensors solve particularly demanding, so far unresolved tasks. At the same time, they are easy to handle.

On the one hand, the sensitivity of the receiver was increased to allow measurements on extremely light-absorbing surfaces. So far low reflectivity materials, such as black paper or rubber, and also highly glossy surfaces, such as plastic parts or varnished sheet metal, were a major challenge. Now the new OADM 13 sensors can be used for applications with these conditions. They are able to process object reflectivities down to 0.5 %.

On the other hand, the software was optimized to a very high ambient light immunity of more 100 kLux. Thus, reliable measurements can be guaranteed under any condition. Additionally, the measuring accuracy at color transitions, e.g. at print products or oxidized surfaces, was considerably increased through improved optics. The new laser sensors work with a very fine linear beam, which also facilitates measurements of small objects. The measuring distance of the very compact sensor is 50 to 200 mm at a resolution of up to 15 ?m.

The sensors can be used in handling applications during semiconductor production where the fine laser beam is an advantage. In the graphics industry or in metal and sheet metal working the improved measuring accuracy at color transitions as well as the sensitive receiver provide the basis for more reliable measurements.

 

Number of letters (including spaces): approx. 1561
This photo is released for publication with this picture.

Press contact

Stefan Diepenbrock
Manager Public Relations
Phone +41 52 728 17 63
Fax +41 52 728 11 44
sdiepenbrock(at)baumer.com
http://www.baumer.com

17.01.2011
Baumer Group