How does an ultrasonic sensor work?

Ultrasonic sensors reliably detect or measure distance within a defined measuring range without contact, no matter which object properties and ambient conditions, e.g. presence of dust, dirt. Ultrasonic sensors emit high-frequency sound waves to measure the time elapsed until being reflected by the object and returning to the sensor. The time measured is used to calculate the distance between sensor and object on the basis of the sound wave travel speed. Ultrasonic sensors also detect presence and position of objects. The measuring range of ultrasonic sensors varies depending on the sensor variant and ambient factors; typical ranges vary between a few centimeters and several meters. Key for the measuring range are frequency and amplitude of the ultrasonic waves as well as the transmitter performance and receiver sensitivity.

Here you will encounter our ultrasonic sensors for object detection as well as all ultrasonic distance sensors and ultrasonic sensors for level measurement.


Sensor principles and structure of ultrasonic sensors

Most ultrasonic sensors are based on the principle of measuring the propagation time of sound between send and receive (proximity sensor). The barrier principle determines the distance from the sensor to the reflector (retro-reflective sensor) or to an object (through-beam sensor) in the measuring range.

More application examples

Ultrasonic proximity sensors

Design and operation

A special sonic transducer is used for the ultrasonic proximity sensors, which allows for alternate transmission and reception of sound waves. The sonic waves emitted by the transducer are reflected by an object and received back in the transducer. After having emitted the sound waves, the ultrasonic sensor will switch to receive mode. The time elapsed between emitting and receiving is proportional to the distance of the object from the sensor.

Ultrasonic proximity sensors integrate transmitter and receiver in the same housing.
Digital output

Sensing is only possible within the detection area. The required sensing range can be adjusted with the sensor's potentiometer or by electronic Teach-in (Teach-in button or remote Teach-in). If an object is detected within the set area, the output will change state which is visualized by the integrated LED.

Target detection

Sonic waves are best reflected from hard surfaces. Targets may be solids, liquids, granules or powders. In general, ultrasonic sensors are deployed for object detection where optical principles would lack reliability.

Standard target

The standard target is defined as a square flat object of following sizes:

The target should be mounted perpendicular to the axis of the sensor.

Size

To ensure a reliable object detection, the reflected signal must be large enough. The intensity of the signal depends on the size of the object. Using a standard object, the full scanning distance Sd is available.

Surface

Detection of sound absorbent materials will result in a reduction of the maximum sensing distance. The maximum sensing distance can be achieved as long as the maximum roughness of the object does not exceed 0,2 mm.

Typical sound absorbing materials are:
 
Sonic cone profiles

The sonic cone profile charts as found in the spec sheets of this catalog represent the active sensing areas for ultrasonic sensors. The charts demonstrate the short-range sonic side lobes, which widen the sensor's close-range aperture angle. Due to sound absorption and air diffusion, the lobes decrease at longer ranges. Size, shape, surface properties and the direction of target detection have very high influence on the lateral detecting region of an ultrasonic sensor. Sonic cone profiles apply to the whole product family, e.g. a 100 - 1000 mm profile is representative for all related sensors of the same sensing range - digital or analog outputs, etc.

Typical sonic lobe of an ultrasonic sensor with measuring distance of up to 1000 mm.
Measuring method
How to determine the sonic lobe of an ultrasonic?

Standard square targets made of steel are used to determine the shape of typical sonic cone profiles.

The targets are positioned perpendicularly to the sensor's reference axis, approached sideways at different distances. The sonic cone profile is then plotted by connecting the measured points with a line. The cone shape can vary if round or differently shaped objects are detected.


Ultrasonic retro-reflective sensors

Design and operation

The retro-reflective ultrasonic sensor is similar in operation to the ultrasonic proximity sensor. The distance from the sensor to the reflector or to an object within the sensing distance is determined by measuring the propagation time. Any sound reflecting, stationary object can be used as a reflector. The sensing distance Sd (distance sensor-reflector) can be adjusted to the set up conditions with the sensor's potentiometer. As long as the measured propagation time of the ultrasonic signal corresponds to the distance from the sensor to the reflector, the device is in the non-active state. When an object comes within the sensing distance, the propagation time changes and the sensor changes to the active state. This also allows detection of sound absorbent and sound deflecting objects.

Ultrasonic retro-reflective sensor with reflector to reflect the ultrasonic signal.
Object detection
Standard object/reflector

The standard target is defined as a square, level object with an edge length of 30 mm (Sde > 1000 mm: 100 mm edge length, Sde ≥ 2500 mm: 300 mm edge length) which is perpendicular to the sensor reference axis. The reflector must be made of a material with good sound reflection properties and be at least the same size as the target.

Advantages
Benefits of ultrasonic retro-reflective sensors.

Ultrasonic through-beam sensors

Design and operation

The emitter and the receiver are in two separate housings. The continuous signal by the emitter is picked up by the receiver. An object interrupting the sonic beam will make the receiver react by giving an output signal. The user may adjust the amplification of the input signal where required. When an object interrupts the sonic beam, the receiver will react and give an output signal.

With the help of the built in potentiometer, the user can adjust the amplification of the input signal, as necessary. 

The state of the output stage as well as the signal intensity are indicated by an LED.

Ultrasonic through-beam sensors accommodate transmitter and receiver in separate housings.
Sonic beam angle α

The sonic beam angle (α) defines the boundaries of the emitted conical beam of the ultrasonic through-beam sensor.

Repeatability

Due to the narrow angle of the sonic beam the repeatability of the switching point of two successive targets, under identical conditions, is better than 3 mm.

Hysteresis

Hysteresis is the difference between the operating point (S1) and the release point (S2). If an object interrupts the sonic beam, the signal level must be increased by about 75 % in order to reset the output signal. Objects which follow one another in quick succession can therefore be easily detected.

Importance of hysteresis utilized by ultrasonic through-beam sensors.

Ultrasonic distance sensors

Design and operation
Function and measuring range of ultrasonic distance sensors.

The sensor provides a distance proportional analog current or analog voltage output, allowing simply applied, non-contact distance measurement. Based on the pulse echo technique, the measured distance value is output as a voltage value.

With distance measuring sensors, the output current or the output voltage is proportional to the distance of the object to be detected. The steepness of the output curve can be modified, depending on the sensor, via a potentiometer, teach-in or qTeach and optimally adapted to the respective application. Applications having long cable runs where there might be EMI or RFI interferences, should use sensors with an analog current output.


Where are ultrasonic sensors used?

Ultrasonic sensors are the allrounders in the world of sensors and are suitable for virtually any detection tasks in industrial applications. The objects to be detected can be solid, liquid, granular or in powder form. They reliably detect transparent or high gloss objects as well as objects of changing color. Being extremely tolerant to dirt, the efficiency of ultrasonic sensors comes into its own especially in harsh working environments, as process reliability is not adversely affected by dust, smoke, mist or similar.

Thanks to their application versatility, ultrasonic sensors are used in most varied industries, such as packaging, electronics and feeder technology. Here you find more application examples of ultrasonic sensors and specific application benefits in specific applications.

Typical applications of ultrasonic sensors

Ultrasonic sensors detect transparent objects and determine the distance to the object.

Reliable detection of various carrier materials, no matter which color, whether glossy or transparent.

Reliable object detection by ultrasonic sensors of any object.

Reliable object detection on varied surface structures.
Level detection in containers and tanks with ultrasonic sensors.

Point level detection of materials with different geometries as well as level detection.
Let us support you

To the products

To the top