In order to be able to design the site optimally and continuously improve it, we use cookies. Among other things, these cookies also collect data on your usage behaviour. If you do not agree, please deselect this option in the "Statistics and Marketing" field below. You can withdraw your consent informally at any time. Further information on this and your rights in connection with the integration of cookies can be found in the data protection declaration.
Mandatory
These cookies are required only to ensure the functionality of the site.
Statistic/User tracking
Storing behavioral user data for analytical purposes and statistics.
An emitter in a separate housing transmits the light to a separate receiver. The object is detected when it breaks the emitted beam.
The active area (A) of a through beam sensor is equal to the diameter of the lens of the receiver or emitter. The acceptance zone (B) of the emitter and receiver is larger. However, this is only important for adjustment and for operation close to glossy surfaces. With focused through beam laser sensors, the active area is the diameter of the laser beam if this is smaller than the receiver lens or the front opening at the receiver end.
Characteristics and advantages
Due to the separated configuration, long ranges with large signal excess gain can be achieved in comparison with equivalent retro-reflective systems. Through beam-sensors are therefore most suitable for operation in unfavorable ambient conditions such as dirt, dust and moisture.
The clearly defined, consistent active zone permits highly constant repeatability throughout the entire sensing distance.
The switching point is independent of the surface properties of the object.
Mounting and adjustment
The emitter and receiver must be aimed at each other. The narrower the angle of radiation and reception, the more accurately this must be conducted.
Retro-reflective sensors
The emitter and receiver are installed in the same housing. The emitted infrared, red or laser light is returned by a triple reflector or a reflective film to the receiver. The output changes its state when the object breaks the light beam (sensor receives no light).
Characteristics and advantages
Single-lens optics Because the emitted and received beams are on the same axis, the direction of approach of the object is irrelevant, and it is possible to look through small openings. Reflectors can also be used in close-range without signal breakdown
Short response times Retro-reflective laser sensors with response times of 0,05 ms and focused laser beams correctly detect the smallest, fast-moving objects (0,1 mm in diameter).
Mounting and adjustment
Each sensor has a separate excess gain curve. As the operating reliability depends heavily on the ambient conditions, it must be ensured that the sensor operates with the highest possible excess signal gain.
Light barrier without reflector
SmartReflect
Contrary to diffuse or through beam sensors, SmartReflect light barriers feature a closed light beam which is set up between the sensor and machine. The sensor switches when an object interrupts the light beam. The only requirement is the presence of a defined background, e.g. a machine part, within the sensing range of the sensor, which closes the light beam.
Characteristics and advantages
Maximum security
Most secure object detection due to the barrier principle
Higher process reliability by eliminating the reflector as the weak spot
No functional impairment due to contamination
Reduced operating costs
Time savings during installation, as no separate reflector / receiver is necessary
No regular reflector exchange necessary
Expensive reflector cleaning is not required
Mounting and adjustment
The SmartReflect light barrier has to be aligned with a machine part within its sensing range. This machine part is then set using the teach-in.
Diffuse sensor with background suppression
By using the triangulation principle, diffuse sensors with background suppression not only measure the light intensity reflected by the target, but also determine the distance of the object from the sensor. In this way, objects with the minimum size of the light beam located within the adjustable sensing distance can be detected regardless of their color and surface.
The diffuse sensors with background suppression and laser light source were developed specifically for applications in which exact positioning is important. With the precisely focused beam, even very small objects such as the wires of a resistor or threads can be clearly detected or counted.
Characteristics and advantages
Adjustable sensing distance The switching point can be adjusted accurately between the object and the interfering background using a set screw or Teach-in method
Largely independent of color The sensing distance remains constant even if the color of the objects changes. Readjustment is therefore unnecessary. Objects changing in the background also have no effect.
Small spot size Laser sensors can detect objects with a size of just 0,1 mm. Sensors with pinpoint diodes have a spot of only 2 mm diameter at the focus.
Red light emitters Visible red light permits simple adjustment of the sensor to small objects by eye.
Short response time Small, quickly moving objects are reliably detected due to the short response time.
Mounting and adjustment
The diffuse sensor must be aimed at the object. The sensing distance must be set to a distance between the target and the background. The background must be located behind the adjusted sensing distance by at least the distance of the sensing distance reduction of the sensor to black.
Diffuse sensors with intensity difference
The emitter and receiver are in the same housing. The emitted infrared, red or laser light is reflected directly by the target back to the sensor. If the target reflects sufficiently well, the received light causes the sensor to switch.
The light shining on the target is largely diffused and reflected back in all directions. A very small part of this remitted light is observed by the receiver. If the target reflects sufficiently well, the received light causes the sensor to switch. As the sensor operates with the reflection from the materials, the surface properties, color and gloss have a great influence on the switching distance.
Characteristics and advantages
Suitable to discern black and white
Relatively large active range
The sensing distance depends largely on the reflective properties of the object surface
Positioning and monitoring with just one sensor
Easy installation
Short response time
Mounting and adjustment
With diffuse sensors operating by the intensity difference principle, the relative receiving signal is specified. This represents the signal level received from a white object as a function of the distance.
Retro-reflective sensors for transparent objects
The emitter and receiver are installed in the same housing. The emitted infrared, red or laser light is returned by a triple reflector or a reflective film to the receiver. The output changes its state when the object breaks the light beam (sensor receives no light).
A polarizing filter permits the emitted light to pass in only one polarization plane. The triple reflector depolarizes the light on reflection. A part of the light reflected back to the receiver passes the second polarization filter, offset by 90°, and is detected by the receiver.
Characteristics and advantages
Polarizing filter Polarizing filter allow objects to be detected regardless of the texture and color of the surface. Glossy and reflective objects are also reliably detected.
Transparent objects Reliably detect transparent objects such as packaging films, PET bottles and glassware.
Mounting and adjustment
Each sensor has a separate excess gain curve. As the operating reliability depends heavily on the ambient conditions, it must be ensured that the sensor operates with the highest possible excess signal gain.