The sequencer enables the possibility of image series recording including automated re-parameterization of the camera based on different events and signals. Therefore the desired camera settings for each step are stored in so-called sequencer sets. Stringing together a number of these sequencer sets results in a sequence. The connection of sequences is done by using different paths. Alongside the camera features the path related features are also part of a sequencer set.


Sequencer sets

Sequencer sets combine camera features – comparable with a user set – and sequencer (set and path) related parameters.

Settings for several camera features such as

can be controlled by the sequencer and thus stored to a sequencer set as well as information for the set switch-over via four different paths.

Each path involves

As with user sets the camera’s current settings are overwritten once a sequencer set is loaded and the sequencer is activated.

VT_Structure_of_a_sequencer_set.png
Structure of a sequencer set

Configuration

In order to avoid overwriting current camera settings while configuring a sequencer, the camera needs to be set to the sequencer configuration mode. Once the camera is set to the sequencer configuration mode, the individual sequencer sets can be selected via the SequencerSetSelector, configured and saved by executing SequencerSetSave. Starting the configured sequence requires to switch the sequencer configuration mode off and to enable the sequencer mode.


Command overview

 

Features

Values

Description

SequencerMode

On/Off

Enables / disables the sequencer mechanism

 

To use this feature, the SequencerConfigurationMode must be off.

SequencerConfigurationMode

On/Off

Enables / disables the sequencer configuration mode

 

Here the sequencer configuration can take place but there is no image acquisition.

 

To use this feature, the SequencerMode must be off.

SequencerFeatureSelector

ExposureTime

Gain (All)

OffsetX

OffsetY

Width

Height

UserOutputValueAll

UserOutputValue

CounterEventSource

CounterEventActivation

CounterResetSource

CounterResetActivation

CounterDuration

TriggerMode

Selects the camera features that are controlled by the sequencer.

SequencerFeatureEnable

true/false [RO]

Enables / disables the selected feature.

SequencerSetSelector

0…127

Selects the sequencer set that contains the feature settings coming afterward.

SequencerSetSave

 

Stores the current device settings to the selected sequencer set.

SequencerSetLoad

 

Loads the currently selected sequencer set.

SequencerSetActive

0…127 [RO]

Displays the currently active sequencer set.

SequencerSetStart

0…127

Defines the initial sequencer set.

SequencerPathSelector

0…3

Selects the path that contains the settings coming afterward.

SequencerSetNext

0…127

Defines the Set, that will be next

SequencerTriggerSource

Counter1End

Counter2End

ExposureActive

Line0

ReadoutActive

Timer1End

Off

Defines the internal or external event that is used as trigger source for the sequencer.

SequencerTriggerActivation

RisingEdge

FallingEdge

AnyEdge

Defines the signals edge that triggers the sequencer.

 

 

 

The grey marked features are only available in the sequencer configuration mode.

 


Related topics

 

In alto