Afin de pouvoir concevoir le site de manière optimale et de l'améliorer continuellement, nous utilisons des cookies. Entre autres choses, ces cookies collectent également des données sur votre comportement d'utilisation. Si vous n'êtes pas d'accord, veuillez désélectionner cette option dans le champ "Statistiques et marketing" ci-dessous. Vous pouvez retirer votre consentement de manière informelle à tout moment. Vous trouverez de plus amples informations à ce sujet et sur vos droits en ce qui concerne l'intégration de cookies dans la déclaration de protection des données.
nécessaire
Ces cookies sont nécessaires pour assurer le bon fonctionnement du site.
Statistiques/Marketing
Stockage des données comportementales des utilisateurs à des fins d'analyse et de statistiques.
When the flow sensor is installed in the higher-level machine, the following must be observed regarding the mounting location:
The flow sensor is not subjected to excessive vibrations at the mounting location
The mounting location allows the proper grounding of the flow sensor
The mounting location allows the proper electrical connection of the flow sensor
For other key prerequisites for mounting the flowmeter, please see the operating manual. It is available in the download section of the product.
Installation position of the flow sensor
Prior to mounting the flow sensor, the flow direction at the mounting location must be determined. The flow direction through the flow sensor is indicated on the name plate. The flow direction is defined as follows:
Positive flow direction: from – to + Negative flow direction: from + to –
Change in the flow direction If the flow direction is changed for system-related reasons, the flow sensor does not have to be dismantled. Only the plus/minus signs of the KA parameters in the BCP operating software must be changed.
When the flow sensor is mounted in a pipe system, inlet and outlet paths must be included. This compensates for interference from curves, valves, pumps, reductions, and similar. Locking and adjusting elements should never be placed directly in front of the flow sensor.
Example:
The following should be observed regarding the installation position of the flow sensor:
The flow sensor must be installed in such a way that the measurement pipe is always completely filled.
When the flow sensor is installed vertically, installation in an ascending pipe is preferable. If required, consult us before installing the sensor in a descending pipe.
Use anti-vibration compensators when installing the flow sensor in long pipes.
Comply with the inlet and outlet paths when installing the flow sensor before or after curves, valves, reductions etc.
The following installation positions are to be avoided:
Do not mount directly before a descending pipe.
Do not mount in a descending pipe.
Do not mount directly before a pipe outlet.
Do not mount on the inlet side of a pump.
Do not mount at the highest point of a pipe system.
Commissioning
All system parameters must be set before commissioning. The flow meter can be configured and operated via the BCP operation software or via the display for the versions PF75H/S. The functions and settings are identical, and both menus have a similar structure.
For more information about the installation and operation of the BCP software, see: www.baumer.com/c/42379