Thanks to linearized calibration curves and very low standard dispersion rates, the new distance-measuring inductive sensors IR08, IR12 and IR18 from the Baumer AlphaProx family offer easy and reasonably priced ...
Quality meets economy – with the new product families U500 and UR18 Baumer sets the highest standards in ultrasonic sensor technology. The sensors for distance measurement and object detection are characterized by...
Baumer has extended the flexible and cost-effective OptoPulse® EIL580 encoder family and has presented additional variants with the attachment forms EURO flange B10 and square flange.
Among the Baumer Hübner Berlin employees are some real running enthusiasts, who took part in the "5x5 km Team Relay Race" held every year under the patronage of the Berlin Waterworks.
With the HOG 86+FSL version, the HOG 86 family of incremental heavy duty encoders by Baumer offers a new version with a mechanical centrifugal switch.
The Baumer CX.I cameras with their outstanding performance convinced the expert panel and participants of the online poll on the inspect award 2019 and were awarded 1st prize in the Vision category.
Precondition for maximum travel convenience is excellent control quality, which in turn is solely ensured by high signal accuracy output by the feedback encoder at the lift motor.
The Baumer optoelectronic sensors O200 are the first miniature sensors on the market to offer 3D CAD data with integrated beam path. This saves valuable time in the engineering process, which previously was quite an effort when integrating the beam path from data sheets.
With their FlexFlow family of flow and temperature sensors, Baumer has expanded their process sensor portfolio. Based on the calorimetric measurement principle, the FlexFlow family...
With the new O300 and O500 sensors in hygienic and washdown design, Baumer offers maximum reliability, comfort and minimum operating costs.
Five new models with a 10 GigE Vision compliant interface for use with optical cables expand the Baumer LX series. The cameras are ideal for applications requiring a high bandwidth of 1.1 GB/s over long distances. In accordance with the SFP+ module used, long-distance solutions can be achieved up to 10 kilometers – without the need for media converters.
The first time this year, the rowing competition in the German city of Krefeld was joined by three teams of Baumer hhs. One male, female and mixed rowing team stood out by performance...
Inductive marine sensors by Baumer were specifically developed for use in harsh environments. In order to minimize the planning work involved in the development phase for onshore and offshore system manufacturers...
The CX.I cameras’ outstanding performance and optimized combination of mechanical and electrical capabilities have convinced the expert jury of the inspect award 2019 as well as the readers of the inspect and messtec drives Automation magazines and for this, they were awarded 1st prize in the vision category.
The absolute motor feedback encoders EFL580 BiSS C by Baumer ensure excellent signal quality thanks to high-precision mechanics and optical sensing.
What is the most efficient way to acquire rotation angles? It’s the Baumer magnetic absolute encoder series EAM580/360. Their precision is unrivalled; no product of another brand can compete in terms of robustness and longevity at this high level...
New, non-contact and fully encapsulated EB360 has been particularly designed for demanding tasks and is wear-free even in harsh environments.
Regularly, the Chamber of Industry and Commerce in Berlin recognizes companies that stand out by particularly qualified trainee programs and apprenticeships.
The sensor specialist Baumer is investing in its future with a new building in Stockach on Lake Constance (near to Constance) in Southern Germany. At the Stockach...
With the new generation of universal temperature transmitters, FlexTop 2212 and 2222, Baumer is expanding its proven range of products. With integrated micro-USB port, automated cable compensation and ...
Thanks to four power outputs which can be triggered individually, the CX.I and LXT cameras allow for quick, easy and cost-efficient 3D surface inspections and identify even slightest non-compliance in structure and shape. Read our technical article on shape from shading and find out how it works.
The new DSRK strain probe from Baumer is setting new standards in tie bar strain measurement. Retaining the excellent measuring performance of its predecessor...
Measuring edge positions, object or column widths are important tasks in the part inspection process.
The new O300 miniature laser sensors with IO-Link by Baumer are the specialists for the reliable detection of very small objects and gaps. Thanks to a laser beam which focuses to within 0.1 mm and...