Baumer is equipping 25 camera models of the LX and CX series with the Precision Time Protocol (PTP) according to the IEEE 1588 Standard, in support of precise time synchronization in Ethernet networks. This allows applications to benefit from all advantages of a PTP-supported inspection system.
Baumer is pleased to announce the immediate availability of LBFH and LBFI level switches with IO-Link and ATEX approval. The IO-Link interface allows the user to automate...
The new O300 miniature laser sensors with IO-Link by Baumer are the specialists for the reliable detection of very small objects and gaps. Thanks to a laser beam which focuses to within 0.1 mm and...
Once again, the excellent credit standing and stable economic business development of Baumer has been certified by Bisnode in their D&B Rating certificate. In the course of the past 12 months, Baumer ranked repeatedly in the lowest risk category. Only 2% of all Swiss companies obtain access to the certification.
The sensor specialist Baumer is investing in its future with a new building in Stockach on Lake Constance (near to Constance) in Southern Germany. At the Stockach...
The new Baumer High-Tech Center at Lake Constance in the German city of Stockach takes shape and has reached the next milestone. In an official ceremony, Baumer celebrated the completed shell...
Shorter and shorter product life cycles, wider product portfolios, increasing customer demands for individualization – these are the challenges facing manufacturing companies today.
The new high performance OM70 laser point and laser line distance sensors from Baumer combine high-precision measurement technology and easy handling in the automation industry.
Baumer has added a new model to its range of CombiLyz conductivity meters. In addition to the compact AFI4, the AFI5 version with remote sensor is now also available.
The absolute motor feedback encoders EFL580 BiSS C by Baumer ensure excellent signal quality thanks to high-precision mechanics and optical sensing.
Precondition for maximum travel convenience is excellent control quality, which in turn is solely ensured by high signal accuracy output by the feedback encoder at the lift motor.
The Baumer optoelectronic sensors O200 are the first miniature sensors on the market to offer 3D CAD data with integrated beam path. This saves valuable time in the engineering process, which previously was quite an effort when integrating the beam path from data sheets.
Baumer awarded and appointed „Preferred Supplier“
In many respects the requirements in the elevator industry are extremely high: maximum transportation comfort, minimal costs and zero defect tolerance during operation in the harshest environments.
When it comes to tough outdoor use, many sensors reach their limits. Inclination sensors by sensor expert Baumer stand for maximum reliability and durability even in a harsh environment.
Whether in industrial environments or in rough outdoor use – increasing of efficiency, reliability and durability are of primary importance.
The Baumer CX.I cameras with their outstanding performance convinced the expert panel and participants of the online poll on the inspect award 2019 and were awarded 1st prize in the Vision category.
Encoder expert Baumer has further expanded their HeavyDuty encoder portfolio. Newcomer POG 86E concentrates on the essential: pure function in corrosion-proof aluminium housing.
With the new PP20R family of pressure sensors, Baumer is expanding its portfolio to offer an attractively priced solution for demanding applications within the rail industry.
Baumer further expands their unparalleled portfolio of HeavyDuty encoders. The new absolute encoder series HMG 10 and PMG 10 merge in their revolutionary design the practice-proven concept...
The CX.I cameras’ outstanding performance and optimized combination of mechanical and electrical capabilities have convinced the expert jury of the inspect award 2019 as well as the readers of the inspect and messtec drives Automation magazines and for this, they were awarded 1st prize in the vision category.