Baumer further expands their unparalleled portfolio of HeavyDuty encoders. The new absolute encoder series HMG 10 and PMG 10 merge in their revolutionary design the practice-proven concept...
Baumer sets new standards in encoder engineering by own freeware for easy encoder testing and parameterization.
The measurement of object height is an important aspect in quality control applications. With the PosCon HM light-section sensor, Baumer offers a unique, compact measuring device for this kind of tasks.
Baumer Group has earned recognition as a Partner-level supplier in the John Deere Achieving Excellence Program. The Partner-level status is Deere & Company’s highest supplier rating.
Capacity, passenger comfort and safety are decisive requirements in railway transport. For many years, Baumer has been proving a reliable partner in the railway industry and...
Baumer has been selected as a recipient of a John Deere supplier innovation award for 2015. The award is presented to a select group of suppliers who have demonstrated innovation...
To meet the ever-growing customer demands for fast supply and adherence to delivery dates, the Baumer focus is on centralized and automated logistics. The ultra-modern logistics center which is part of...
The new O200 sensors from Baumer considerably raise the performance bar for optical miniature sensors. Economical in operation and featuring an impressive function variety in a standardized miniature housing...
Five new models with a 10 GigE Vision compliant interface for use with optical cables expand the Baumer LX series. The cameras are ideal for applications requiring a high bandwidth of 1.1 GB/s over long distances. In accordance with the SFP+ module used, long-distance solutions can be achieved up to 10 kilometers – without the need for media converters.
The Baumer CX.I cameras with their outstanding performance convinced the expert panel and participants of the online poll on the inspect award 2019 and were awarded 1st prize in the Vision category.
To count, measure, detect – the tasks of Baumer sensors in machinery and installations are very clear. But there is much more to the small power packs. Many Baumer sensors feature IO-Link, a fast communication interface that besides measured values transmits a great bunch of additional information...
The new distance measuring inductive sensors AlphaProx with IO-Link interface from Baumer offer more than precise measurement technology. In addition to micrometer-precise distance values, two switching points...
We are talking with Lina De Windt today. She studies electrical engineering at ETH in Zurich and is an electrical engineer on the Swissloop team. In the interview, she tells us how she overcomes challenges in the testing phase with her team, how important team spirit is for this, and how successes are celebrated.
The CX.I cameras’ outstanding performance and optimized combination of mechanical and electrical capabilities have convinced the expert jury of the inspect award 2019 as well as the readers of the inspect and messtec drives Automation magazines and for this, they were awarded 1st prize in the vision category.
With the new O300 and O500 sensors in hygienic and washdown design, Baumer offers maximum reliability, comfort and minimum operating costs.
Thanks to four power outputs which can be triggered individually, the CX.I and LXT cameras allow for quick, easy and cost-efficient 3D surface inspections and identify even slightest non-compliance in structure and shape. Read our technical article on shape from shading and find out how it works.
With its O200 photoelectric miniature sensors, Baumer offers a new dimension in terms of reliability, speed and range for confined machine installation spaces. Thanks to their increased functional reserves, the O200 diffuse sensors with background suppression are the only ones with up to 120 mm sensing distance even on darkest and shiny objects such as mobile phone housings.
The O300 and O500 SmartReflect Transparent sensors set new standards in the detection of transparent objects. The light barrier without a reflector is the only sensor in its class ...
Inductive marine sensors by Baumer were specifically developed for use in harsh environments. In order to minimize the planning work involved in the development phase for onshore and offshore system manufacturers...
Typically high shaft loads and situation-induced axial impact or overloads in shaft copying systems present a real challenge to encoders.
The O200 photoelectric miniature sensors from Baumer with IO-Link interface are the ideal solution for the detection demanding objects in confined spaces. With their unique ambient light immunity and their precise, reproducible and color-independent switching distances, the comprehensive portfolio offers absolute reliability even under difficult conditions.
With the new AlphaProx IR12 and IR18 High Sensitivity sensors, Baumer is offering a true worldwide innovation: the first teachable standard inductive sensors for measuring tiny changes in position.
Baumer PosCon HM is a unique, compact measuring unit for the intelligent height measurement of objects with 5 key figures.
In many respects the requirements in the elevator industry are extremely high: maximum transportation comfort, minimal costs and zero defect tolerance during operation in the harshest environments.
With the new generation of universal temperature transmitters, FlexTop 2212 and 2222, Baumer is expanding its proven range of products. With integrated micro-USB port, automated cable compensation and ...
The Baumer LX VisualApplets cameras with integrated image preprocessing and the VeriSens vision sensors with Color FEX 3D color assistant were awarded as inVISION Top Innovations 2016.
The Baumer LX VisualApplets cameras with integrated image preprocessing were honored with the highest award at this year‘s „Vision Systems Design Innovators Awards Program“.