The Baumer LX VisualApplets cameras with integrated image preprocessing were honored with the highest award at this year‘s „Vision Systems Design Innovators Awards Program“.
To count, measure, detect – the tasks of Baumer sensors in machinery and installations are very clear. But there is much more to the small power packs. Many Baumer sensors feature IO-Link, a fast communication interface that besides measured values transmits a great bunch of additional information...
The new smart VeriSens vision sensors XF900 and XC900 control the collaborating robots (cobots) of Universal Robots within only a few minutes of setting up. The robot-compatible vision sensors are mounted directly on the cobot or above it. Thanks to the SmartGrid (patent pending), calibration in terms of image distortion, conversion into world coordinates, and coordinate alignment between the vision sensor and robot take place automatically and extremely easy.
Inductive marine sensors by Baumer were specifically developed for use in harsh environments. In order to minimize the planning work involved in the development phase for onshore and offshore system manufacturers...
The CX.I cameras’ outstanding performance and optimized combination of mechanical and electrical capabilities have convinced the expert jury of the inspect award 2019 as well as the readers of the inspect and messtec drives Automation magazines and for this, they were awarded 1st prize in the vision category.
Progressive digitization and the trend towards individualized products also require solutions that are flexible and as automated as possible, even in the part inspection area.
The new high performance OM70 laser point and laser line distance sensors from Baumer combine high-precision measurement technology and easy handling in the automation industry.
Laser distance sensors enable high-precision distance and position measurement with a resolution of less than one micrometer. In practice, however, there are interference effects that can reduce the repeatability of optical distance measurements.
The O200 photoelectric miniature sensors from Baumer with IO-Link interface are the ideal solution for the detection demanding objects in confined spaces. With their unique ambient light immunity and their precise, reproducible and color-independent switching distances, the comprehensive portfolio offers absolute reliability even under difficult conditions.
At the recent „Vision Show“ in Boston, the Baumer SmartApplets have been awarded bronze under the "Vision Systems Design 2018 Innovators Awards Program". These ready-to-use function extensions for the LX VisualApplets cameras provide users with the benefit of drop-in solutions for standard tasks...
The Baumer LX VisualApplets cameras with integrated image preprocessing and the VeriSens vision sensors with Color FEX 3D color assistant were awarded as inVISION Top Innovations 2016.
With FLEX-3A, OTTO Vision Technology GmbH offers a high-end 3D scanner with a measuring range from 20 mm to 200 mm for non-contact 3D detection and geometry inspection of complex objects. Find out in our application report which is the role played by two cameras of the CX series with 12 megapixel and USB 3.0 interface.
With the new PP20R family of pressure sensors, Baumer is expanding its portfolio to offer an attractively priced solution for demanding applications within the rail industry.
Where do manufacturers in machinery and plant engineering get the best optical sensors, level switches and rotary encoders from? Answer: from Baumer. Customers know well that at Baumer they always get some extra performance on top as special support in tricky measuring tasks.
Inductive sensors very often form the basis for the reliable control of machines and systems.
In applications where non-ferrous metals such as aluminum need to be detected at the same working distance as steel, Factor 1 inductive sensors are a perfect fit. Baumer offers a unique selection of such sensors in switching and measuring versions.
The Baumer CX.I cameras with their outstanding performance convinced the expert panel and participants of the online poll on the inspect award 2019 and were awarded 1st prize in the Vision category.
With the expansion of the LX series by eight new models, Baumer combines the latest Sony Pregius sensors with the innovative, cost-effective 10 GigE interface.
When it comes to tough outdoor use, many sensors reach their limits. Inclination sensors by sensor expert Baumer stand for maximum reliability and durability even in a harsh environment.
Hyperloop, the project brought into being by Elon Musk, aims at revolutionizing mobility. Similar to the principle of pneumatic tube transport, people or goods travel without resistance and...
Quite many sensors meet their limits when it comes to measuring angles in harsh outdoor conditions. Inclination sensors in robust industrial design by sensor expert Baumer ensure reliable measurements...
Detecting objects with gaps or holes still constitutes a challenge for optical sensors in factory automation. With its new optical O300 miniature sensors with linear beam...
The possibility of bidirectional communication using the standardized IO-Link interface is the basis for new functions and services in the IIoT era. In addition to the primary function, such as a switching signal, additional secondary data provides valuable information about the production process. Access to the additional information allows the overall effectiveness of the system to be optimized and enables preventative maintenance.
The Baumer optoelectronic sensors O200 are the first miniature sensors on the market to offer 3D CAD data with integrated beam path. This saves valuable time in the engineering process, which previously was quite an effort when integrating the beam path from data sheets.