Bigger container vessels in shorter docking times: still the pressure on crane and hoist equipment is to work 24/7. For more than 60 years Baumer Hübner has been transforming experience in harsh port environments into unmatched robust and durable sensor solutions. Today we offer cutting-edge technology that increases uptime in cranes, hoists, winches and other port equipment whilst boosting IOT developments with intelligent, programmable components.


Port overview

Import containers will be moved from quayside to landside, export containers from landside to quayside and transshipment containers from quayside to the stacks for intermediate storage and back to the quayside. As for the import direction, a vessel arrives with the containers at the allocated berthing place and quay cranes are assigned for discharging.

Port applications at a glance:
Port_hybris_banner_1440x814.jpg

Need advice? Contact us

Port infrastructure

Ship to shore crane

Learn more about the sensor technology and suitable products used on ship-to-shore cranes...
Port_STS ship to shore rendering_banner.jpg

Stacking cranes

Stacking cranes are located in both intermodal and yard areas. Please click on the items below to learn more...

Port_stacking cranes RMG RTG ASC_hybris_banner.jpg

Ship loader / unloader

Port_spreader_hybris_banner.jpg

Stacker reclaimer

A stacker-reclaimer is a combination of a stacker for stacking materials and a reclaimer for recovering bunker material such as ore or grain from a stockpile. It can stack material on stockpiles and reclaim it with a bucket wheel at the tip of the boom.
Por solution page Heavy duty Stacker Reclaimer

Mobile portal crane

Portal or gantry cranes are a type of crane that spans an object or work area, and the entire crane can be moved around the work area.

Mobile cranes are designed to be easily transported to a job site and used with various types of loads and goods with little or no erection or assembly.

Mobile portal cane Port solution page

Deck crane

Deck cranes are located on bulk carriers, container ships as well as engineering vessels and provide safe and effective loading and unloading of cargo on general cargo, container, bulk and other vessels.
Deck crane on a ship - port solution page

STS machinery room

Interior of a ship to shore (STS) machine room.
Port Hoist Winch Ship to Shore (STS) Machinery room

Reach stacker

A reach stacker is a Mobile Machine for handling intermodal freight containers in terminals or ports. They are able to transport quickly over short distances and - depending on access - stack containers.
Port_mobile-port-equipment_reach-stacker_hybris_banner.jpg

Boom extension

Container rotation

Container angle

Hydraulic monitoring

Boom angle

Moving direction

Straddel or van carrier

A straddle carrier or van carrier is a mobile machine for transporting goods that carries / transports its load underneath. Compared to trucks, for example, this means that loading and unloading does not require the help of cranes or forklifts.
Port solution page straddle or van carrier

Hoist

Container handler

A container handler is a special forklift capable of stacking empty containers and dispatching full ones with high precision.
Port_container-handler_0011-bg_hybris_banner.jpg

Lift extension

Stability control

Moving direction

Steering

Automated Guided Vehicle (AGV)

Automated Guided Vehicles (AGVs), self-driving vehicles or autonomous driverless vehicles are material handling or load carrying robots that move autonomously around the port without an operator or driver on board.
Port_AGV_0010-bg_hybris_banner.jpg

Weight detection

Steering

Moving direction

Position determination

Collision detection

Make a difference with your Material handling equipment

Rising labor costs are accelerating the trend toward more automation, process flexibility and performance in material handling equipment. In addition, the changing normative environment is increasing the demand for sensors for safety applications.

Experience why you can make a difference realizing these goals with Baumer sensors.

Know all three reasons

Other topics

Contact

Au sommet