Latest News Archived News
Teaserbilder_Presse_Zchn-6938-1_600x338.jpg

Quality all along the line

Precise, non-contact inline-measurements by optical distance sensors without process interruptions are vital in high-quality product manufacture. In measurements on demanding surfaces such as galvanized or brushed metal, the OM70 laser distance sensors with line beam shape ensure the required reliability. On structured surfaces or colored edges, point laser measurements cause interference and deliver rather inconsistent and little reliable results. 

W-Thema_VT_20190729_Fachartikel-SfS_600x338.jpg

What’s in a shadow?

Thanks to four power outputs which can be triggered individually, the CX.I and LXT cameras allow for quick, easy and cost-efficient 3D surface inspections and identify even slightest non-compliance in structure and shape. Read our technical article on shape from shading and find out how it works.

Baumer_O200-Background-Suppression-20190606-PH.jpg

Best-in-class background suppression in miniature format

With its O200 photoelectric miniature sensors, Baumer offers a new dimension in terms of reliability, speed and range for confined machine installation spaces. Thanks to their increased functional reserves, the O200 diffuse sensors with background suppression are the only ones with up to 120 mm sensing distance even on darkest and shiny objects such as mobile phone housings.

Baumer_O200_CAD-Daten_20190520_teaser1.jpg

Engineering made easy - the world's first photoelectric miniature sensors with CAD data and beam path

The Baumer optoelectronic sensors O200 are the first miniature sensors on the market to offer 3D CAD data with integrated beam path. This saves valuable time in the engineering process, which previously was quite an effort when integrating the beam path from data sheets.

teaser_Baumer_proTect+.jpg

proTect+ sensors from Baumer go beyond IP standard requirements

Rough ambient conditions, regular cleaning cycles - these are daily occurrences which sensors are often exposed to in outdoor, hygienic and washdown applications. Proven IP 68 and IP 69K protection make sensors endure such demanding conditions - tested when new. But what if having been in use in tough field environments for several years?

aumo_news_bild6.jpg

Inspections on 10 million plastic parts per year

The clever inspection system from automation specialist AUMO utilizes ten CX cameras for quality inspections on 10 million socket cover plates per year to check dimensions and outer contours for smallest scratches or surface irregularities. Want to learn more? Read the application report.

autoforce_Bild_teaser.jpg

Image-based, all automated inspection upon blowholes sized 0.4 mm upwards

At Gruber & Kaja High Tech Metals GmbH, a multi-camera system with multi-stage image evaluation ensures that only cavity-free aluminium die cast parts will be delivered. For this purpose, six GigE cameras of the LX series deliver high-resolution images.

Baumer_Inductive-sensors-factor-1_teaser.jpg

Factor 1 inductive sensors by Baumer

Inductive sensors very often form the basis for the reliable control of machines and systems. 

In applications where non-ferrous metals such as aluminum need to be detected at the same working distance as steel, Factor 1 inductive sensors are a perfect fit. Baumer offers a unique selection of such sensors in switching and measuring versions.

Baumer_IO-Link-Optimizing-Teaser.jpg

Optimizing production processes with digital sensor data

The possibility of bidirectional communication using the standardized IO-Link interface is the basis for new functions and services in the IIoT era. In addition to the primary function, such as a switching signal, additional secondary data provides valuable information about the production process. Access to the additional information allows the overall effectiveness of the system to be optimized and enables preventative maintenance.

 

Technical report: Precise image analysis thanks to distortion and shading correction

Correcting distortion, shading and perspective bias in real-time, the VeriSens vision sensors by Baumer are the smart and simple way for precise image evaluation. Read about your application benefits in our specialist article.

Teaserbild_PR_O200.jpg

Extremely reliable detection even with difficult objects - O200 miniature sensors

The O200 photoelectric miniature sensors from Baumer with IO-Link interface are the ideal solution for the detection demanding objects in confined spaces. With their unique ambient light immunity and their precise, reproducible and color-independent switching distances, the comprehensive portfolio offers absolute reliability even under difficult conditions.

Teaserbilder_Presse_E-Zchn-6931_600x338.jpg

Sensors – High-quality standard solution instead of expensive special solutions

Shorter and shorter product life cycles, wider product portfolios, increasing customer demands for individualization – these are the challenges facing manufacturing companies today. 

To the top