Teaserbilder_News_7981_600x338.jpg

U500 and UR18 ultrasonic sensors from Baumer

Ultrasonic sensors are the all-round talents of sensor technology. They are resistant to soiling and allow the reliable detection of objects regardless of the color and surface finish. When it comes to transparent or high-gloss objects in particular, ultrasonic sensors are superior optical sensors. The new product series U500 and UR18 with IO-Link offer even more.
Teaserbilder_News_7129_PL20_600x338.jpg

Clever³ – simpler. More reliable. More intelligent.

The original puts you one step ahead – point level detection has never been this easy and reliable. Thanks to the new level switch PL20, the CleverLevel series from Baumer now offers more possibilities for detecting point levels. CleverLevel reliably detects every type of medium, whether liquid, pasty, viscous, or solid, and is therefore the solution for a variety of applications for which standard vibrating forks are used today. 
Teaserbilder_News_9026_600x338.jpg

An innovation with added value – the PP20H pressure sensor with IO-Link wins the Innovations Showcase Award

At the Process Expo in Chicago, a panel of experts from the food processing industry selected the PP20H pressure sensor as the winner of the Innovations Showcase Award in the dairy product category. The pressure sensor prevailed among the 17 finalists due to its condensate-resistant silicon measuring cell, exceptional precision across the entire temperature range, and IO-Link interface. 
Newsteaser_Ultraschallsensoren.jpg

Going beyond limits: Ultrasonic sensors U500/UR18 feature the shortest blind range at yet long sensing distance available on the market

Thanks to the unique sensor element, the sensor families U500 and UR18 with IO-Link are not only more robust than all comparable sensors on the market, but their extremely short blind range at yet very long sensing distance brings requirements to a whole new level.
3514-0-DCH_600x338px.jpg

Performance redefined: 10 GigE cameras with 3rd generation Sony Pregius CMOS sensors

Greater sensitivity, improved image quality, and frame rates of more than 1500 fps – six new LXT cameras with resolutions from 0.5 to 7.1 megapixels combine 3rd generation Sony Pregius CMOS sensors with 10 GigE, thus allowing considerable performance improvements. With a pixel size of 4.5 or 9 µm, the cameras offer very high sensitivity. This way, they provide better support for applications with a short exposure time or NIR illumination, for example. 
Teaserbilder_News_Baumer_Photo_AFI_PP20H_8933_600x338.jpg

Digital and analog interface benefits all at once thanks to Dual Channel

Digital communication opens up many opportunities – but only sensors that reliably deliver precise measured values offer real added value by IO-Link. Well established and appreciated by many users, both pressure sensor PP20H and CombiLyz AFI conductivity sensor excel by outstanding measuring performance and IO-Link interface, but now they offer even more interesting features such as simple and fast parameterization- even during operation.

To the top