28-nov-2016

The shell of the office building being the first construction section has been finalised

Barely two months after completion of the primary foundation plates, half of the new office building is ready and the workers are busy with preparing the roof. Even the building hosting logistics now presents its roof.

Also works on the production building are rapidly advancing. The first floor has been finished and the base plate for the second floor is being casted. The roof truss is expected to be delivered soon, so that also this building will soon be “covered”. 

Luftaufnahme_20161124_0007_600x338.jpg
Luftaufnahme_20161124_0008_600x338.jpg
Hasta la cima