The radar sensor developed by Baumer enables you to measure the distance of objects over wide distances. Aside from distance measurements, it is also possible to measure the relative speed of the detected object.

The sensor is based on the Frequency Modulated Continuous Wave (FMCW) technology. Here the carrier frequency is constantly modulated within a small range (the bandwidth). As soon as the signal is reflected back from an object, it is possible to measure the distance and the speed of the object through frequency comparison.

The sensor utilizes a very high carrier frequency, this allows to generate a very narrow beam cone. This allows to detect even small objects, without interference from neighbouring objects over large distances.

Allg-Technologiezeichnung_Radarsensoren_EN.png

Teaser_Know-how_E-Zchn-6774_600x338.jpg

Baumer radar sensors operate on the FMCW method (Frequency Modulated Continuous Wave). Here the radar sensor emits a frequency (f) which is continuously changed over time (t). In this way a frequency sweep is created. The difference between minimal and maximal frequency is called bandwidth (Bsweep). 

Teaser_Know-how_E-Zchn-6775_600x338.jpg

The frequency sweep repeats periodically with the sweep time Ts. One modulation type is the sawtooth option as shown in the illustration. As an alternative, triangle wave modulation can be used. The time duration between of this periodically modulation is called sweep time (Ts). During the sweep time, the frequency is continuously increased, e.g. from 122 to 123 GHz.

Teaser_Know-how_E-Zchn-6776_600x338.jpg

When the emitted radarwave hits an object within the radar cone, a portion of the signal is reflected. This can be detected as a echo signal in the radar sensor.

Teaser_Know-how_E-Zchn-6777_600x338.jpg

Due to frequency sweep the echo signal has a lower frequency then the emitted signal. The difference between the current frequency and the received frequency (frequency beat fb) is detected by the radar sensor as measured signal.

Teaser_Know-how_E-Zchn-6778_600x338.jpg

The distance R between radar sensor and object is determined out of the detected frequency sweep (fb), sweep time (Ts) and band width (Bsweep).

Shortcuts:

td = Runtime shift
Ts = Sweep time
R = Range
c = Speed of light
fb = Frequency beat 
Bsweep = Bandwidth


You may also be interested in

To the top