Baumer_SE-AD_Anwendungen_OXM_20230820_AR_DE_Bild3.jpeg

Always keeping an eye on web edges and margins

These all-rounders are underestimated indeed: Smart 2D profile sensors are ready for use in no time and very versatile, for example in edge control. Four smart applications: 
What is the exact object position on the belt? What is its height? Is the edge even? In lots of automated processes, this information is required to ensure smoothly running production. Most common are optical, inductive or ultrasonic sensors sometimes also cameras are deployed to collect such data. A versatile, lesser-known alternative are smart 2D profile sensors. In this report we show four examples where high-performance profile sensors from Baumer are particularly user-friendly and cost-effective solutions. 
Angel Tree and food

Baumer North America launches food and toy drive for the holidays

Not only does Baumer develop technological solutions to improve industrial operations to save resources, but we also actively work with our community and partners to make a difference locally. For Thanksgiving and the Holiday season, employees at Baumer North America launched a food and toy drive to help families in need.
Teaser-Hybris_Baumer_PR_PLP70_AutomationsBest_Award_DE_720x405-bg_screen.png

AutomationsBest Award for Baumer level sensor PLP70

Baumer innovations are well-received, both by users and the professional audience of the trade magazine "messtec drives Automation" (Wiley). The smart level sensor CombiLevel PLP70 has finished first place in the voting for the AutomationsBest Award in the category Best Product. Product manager Julian Budde received the award at SPS 2023 in Nuremberg.
EAM580RS

Robust encoder for maximum safety

The EAM580RS magnetic encoder in certified safety design simplifies engineering in safety-relevant fields of application. The safety encoder was specially developed for harsh outdoor applications and mobile machines and is immune to shocks and vibrations.
Baumer at BrauBeviale

BrauBeviale: Baumer presents sensor solutions for improved efficiency

At upcoming BrauBeviale in Nuremberg (28 - 30 November),sensor expert Baumer will be presenting intelligent sensor solutions for the brewing and beverage industry. The trade show focuses on resource efficiency, which can be significantly increased with smart Baumer products. Further to their core competencies in the field of process sensor technology, Baumer is presenting their high-performance sensor solutions for packaging applications.
Inspect Award 2023

Baumer cameras with integrated cooling pipe win inspect award 2023

Sensor and industrial camera expert Baumer strives to find new ways in order to offer customers measurable added value. A current example from industrial image processing are the industrial cameras of the CX series with integrated cooling pipe. So far, in high temperature environments the camera housing used to be embedded in external cooling components to ensure constant camera temperature. Such effort is time consuming and adds to camera dimensions. To counteract this drawback, Baumer has extended the CX series by cameras with integrated cooling. The patented cooling pipe of the CX.XC cameras space-savingly winds its way inside the camera housing to ensure thermal stability within an instant. 
 
To the top