Together we safeguard processes and keep costs under control
Interactive_Landingpage_heatExchangers.jpg


Fast temperature recording for optimized operation

Fast temperature measurement improves the control loop, helping to ensure quality and reduce energy consumption. The faster the response time of the temperature sensor, the quicker the heating valve can be actuated. This allows a small safety margin, while reducing the temperature level as a whole. As a result, less heat energy is required and the product better retains its taste.
Teaser_2_600x338_V3.png

Sustainable safety

Exact flow measurements ensure that the heat retention time is precisely maintained. The precise flow rate adjustment also allows an overall control concept for increasing the system capacity to be implemented.
Teaser_Zchn-7141_600x338.png

Optimized cleaning management

Highly accurate pressure measurement at the inlet and outlet of the heat exchanger allows accurate predictions about when the heat exchanger needs to be cleaned. The more accurate the sensor, the quicker it reports a pressure drop of the products being treated below that of the heating/cooling medium.
Teaser_1_600x338_V3.png

Built for heat exchanger automation

To the top