Para poder diseñar el sitio de forma óptima y mejorarlo continuamente, utilizamos cookies. Entre otras cosas, estas cookies también recogen datos sobre su comportamiento de uso. Si no está de acuerdo, por favor desactive esta opción en el campo "Estadísticas y marketing" que aparece a continuación. Puede retirar su consentimiento de manera informal en cualquier momento. Encontrará más información al respecto, así como sus derechos en relación con la integración de las cookies, en la declaración de protección de datos.
Obligatorio
Estas cookies son necesarias sólo para asegurar la funcionalidad del sitio.
Estadística/Seguimiento de usuarios
Almacenamiento de datos de comportamiento de los usuarios con fines analíticos y estadísticos.
Baumer ya ha ganado galardones nacionales e internacionales en distintas categorías como innovación, diseño y calidad. Los galardones de distintos jurados especializados son un signo de nuestra calidad y espíritu pionero.
The hygienic pressure sensor PP20H was voted third place in the “Products of the year 2019” in the sensor category by the readers of the professional journal Elektronik. The pressure sensor PP20H with condensate-proof silicon measuring cell in IP69K-rated stainless steel housing meets the requirements of demanding hygienic applications.
Descubra más acerca de nuestros premios en la historia reciente
The CleverLevel PL20 point level sensor from Baumer wins its next trophy. In the vote for Product of the Year, readers of the trade journal Computer & Automation voted the proven process sensor into second place in the sensor category.
With its minimalist and robust design the 360° process visualization Baumer KingCrown has won this year’s Red Dot Award in the Product Design category. The stainless steel electrical connection in combination with the visual status display is distinguished, among other things, by its maximum robustness and long-term tightness according to the Baumer proTect+ tightness concept.
With the help of innovative solutions such as the PAD20, Baumer supports customers in making production processes more efficient and optimizing the use of resources. The PAD20 analysis sensor for the detection of air and gas bubbles is the answer to a decades-old problem in the dairy industry that enables to save resources and expand production capacities.
Quite a start into the new year: Already in November, the automated coordinate alignment between cobot and vision sensor via SmartGrid convinced the readers of the inspect magazine and won the inspect award in the category Vision.
The automated coordinate alignment of the robot-compatible VeriSens XF/XC900 vision sensors from Baumer convinced the expert jury of the inspect award 2021. Out of nine finalist products in the online voting, the sensors were awarded first place in the category Vision.
At the Process Expo in Chicago, a panel of experts from the food processing industry selected the PP20H pressure sensor as the winner of the Innovations Showcase Award in the dairy product category. The pressure sensor prevailed among the 17 finalists due to its condensate-resistant silicon measuring cell, exceptional precision across the entire temperature range, and IO-Link interface.