4 juil. 2023

Baumer cameras with patented cooling concept nominated for inspect award - vote now
Inspect Award Nomination
The Baumer CX.XC industrial cameras with integrated cooling pipe are nominated for the inspect award 2023. Voting runs until 15 September 2023.

As a pioneer in industrial image processing, Baumer creates measurable added value with innovative solutions. A current example is the CX.XC industrial cameras, which enable high-precision image capture and significant time savings thanks to their unique cooling concept with integrated cooling pipe. This allows production throughput to be significantly increased, especially in the semiconductor industry. For the integration of the cooling pipe into the small housing, Baumer uses a special 3D printing process that ensures maintenance-free tightness. The advantages of the innovative cooling system apparently also convinced the jury of the inspect award 2023 of the Wiley-VCH publishing house. The expert panel nominated Baumer CX.XC camera for the inspect award in the "Vision" category. A total of ten innovations were selected in this category. Now readers will decide which innovation will receive the inspect award 2023.

Vote here!

Ideal for wafer bonding and high ambient temperatures
 

The Baumer CX.XC cameras offer numerous user benefits thanks to their integrated cooling pipe. They enable high-precision image capture through thermal stability. At high ambient temperatures, they still work reliably while offering a very compact design. Preferred application fields are in semiconductor manufacturing (e.g. wafer bonding) but also in glass industry or metal processing. More details about the patented cooling pipe. 

Now it is up to the users to choose the best machine vision innovation of 2023. The three candidates with the most votes in each category will receive the coveted trophy at the end.

Vote here


Plus d’informations

Press contact
Au sommet