With the expansion of the LX series by eight new models, Baumer combines the latest Sony Pregius sensors with the innovative, cost-effective 10 GigE interface.
What is the most efficient way to acquire rotation angles? It’s the Baumer magnetic absolute encoder series EAM580/360. Their precision is unrivalled; no product of another brand can compete in terms of robustness and longevity at this high level...
Where do manufacturers in machinery and plant engineering get the best optical sensors, level switches and rotary encoders from? Answer: from Baumer. Customers know well that at Baumer they always get some extra performance on top as special support in tricky measuring tasks.
With FLEX-3A, OTTO Vision Technology GmbH offers a high-end 3D scanner with a measuring range from 20 mm to 200 mm for non-contact 3D detection and geometry inspection of complex objects. Find out in our application report which is the role played by two cameras of the CX series with 12 megapixel and USB 3.0 interface.
Baumer offers the first CMOS cameras with an exposure time down to 1 µs in the mainstream segment of digital industrial cameras. The CX models including the second generation...
To count, measure, detect – the tasks of Baumer sensors in machinery and installations are very clear. But there is much more to the small power packs. Many Baumer sensors feature IO-Link, a fast communication interface that besides measured values transmits a great bunch of additional information...
The new O200 sensors from Baumer considerably raise the performance bar for optical miniature sensors. Economical in operation and featuring an impressive function variety in a standardized miniature housing...
The Ethernet encoders of the EAL580 series by the encoder expert Baumer set new benchmarks in the field of absolute encoders.
Sensor expert Baumer is further expanding their portfolio of cable transducers being the easiest, most reliable and cost-efficient way to measure linear motion within a path from 0.5 to 50 m.
Precondition for maximum travel convenience is excellent control quality, which in turn is solely ensured by high signal accuracy output by the feedback encoder at the lift motor.
The Baumer incremental encoder series OptoPulse® EIL580 presents a new family member with further enhanced protection against inductive shaft currents.
Quite many sensors meet their limits when it comes to measuring angles in harsh outdoor conditions. Inclination sensors in robust industrial design by sensor expert Baumer ensure reliable measurements...
Baumer further expands their unparalleled portfolio of HeavyDuty encoders. The new absolute encoder series HMG 10 and PMG 10 merge in their revolutionary design the practice-proven concept...
Whether in industrial environments or in rough outdoor use – increasing of efficiency, reliability and durability are of primary importance.
The absolute motor feedback encoders EFL580 BiSS C by Baumer ensure excellent signal quality thanks to high-precision mechanics and optical sensing.
Demanding applications in machine and plant construction, for example in handling and assembly, graphic and packaging machines, require high precision in real-time with minimal cycle time and jitter.
Baumer is equipping 25 camera models of the LX and CX series with the Precision Time Protocol (PTP) according to the IEEE 1588 Standard, in support of precise time synchronization in Ethernet networks. This allows applications to benefit from all advantages of a PTP-supported inspection system.
Five new models with a 10 GigE Vision compliant interface for use with optical cables expand the Baumer LX series. The cameras are ideal for applications requiring a high bandwidth of 1.1 GB/s over long distances. In accordance with the SFP+ module used, long-distance solutions can be achieved up to 10 kilometers – without the need for media converters.
When it comes to tough outdoor use, many sensors reach their limits. Inclination sensors by sensor expert Baumer stand for maximum reliability and durability even in a harsh environment.
With the HMG10P / PMG10P series, Baumer raises the bar for HeavyDuty encoder technology. The encoders enable convenient configuration by any input device via WLAN adapter for individual configuration...
The Baumer optoelectronic sensors O200 are the first miniature sensors on the market to offer 3D CAD data with integrated beam path. This saves valuable time in the engineering process, which previously was quite an effort when integrating the beam path from data sheets.
Baumer has extended the flexible and cost-effective OptoPulse® EIL580 encoder family and has presented additional variants with the attachment forms EURO flange B10 and square flange.
With the HOG 86+FSL version, the HOG 86 family of incremental heavy duty encoders by Baumer offers a new version with a mechanical centrifugal switch.
Typically high shaft loads and situation-induced axial impact or overloads in shaft copying systems present a real challenge to encoders.