BAD20 Pump Industry Award

Pump Industry Award 2024: Baumer Bubble Sensor PAD20 named finalist

The innovative Baumer Bubble Sensor PAD20 is on the shortlist for the Pump Industry Award 2024, an international trophy recognizing outstanding achievements within the pump industry. The PAD20 is named finalist as it is a smart solution to protect pumps from running dry and to ensure maximum performance and use of resources.
Baumer_PR__Presse_Feedrate_Control_20231210_720x405.jpg

Smart Radar System wins a Silver Medal in Innovation Awards

A new system allows for combine harvesters to maximize throughput without risking overload and blockages. Centrepiece of this innovative system is the forward-looking radar system by Baumer. The new Advanced Feedrate Control system for Case IH Axial-Flow combines now has been awarded a Silver Medal in the DLG Innovation Awards.

PL240

Il nuovo sensore Baumer rileva i livelli senza subire influenze da pellicole e adesioni

Rilevamento senza contatto delle soglie di livello anche se le pareti interne del serbatoio sono rivestite da micropellicole o presentano residui: il nuovo sensore capacitivo PL240 di Baumer rileva i livelli in modo affidabile, anche in condizioni difficili, grazie al suo principio di misurazione innovativo ed intelligente.
Teaser-Hybris_Baumer_PR_PLP70_AutomationsBest_Award_DE_720x405-bg_screen.png

AutomationsBest Award for Baumer level sensor PLP70

Baumer innovations are well-received, both by users and the professional audience of the trade magazine "messtec drives Automation" (Wiley). The smart level sensor CombiLevel PLP70 has finished first place in the voting for the AutomationsBest Award in the category Best Product. Product manager Julian Budde received the award at SPS 2023 in Nuremberg.
EAM580RS

Encoder robusto per la massima sicurezza delle macchine mobili

Il nuovo encoder EAM580RS di Baumer e stato sviluppato e progettato specificatamente per la sicurezza in applicazioni mobili e outdoor. Con l'aumentare dell'automazione delle macchine mobili cresce anche la necessità di soluzioni sicure, spesso associato a un dispendio economico maggiore. In tal senso può aiutare poter contare su componenti dotati di certificazioni di sicurezza come l'encoder assoluto EAM580RS che contribuisce a ridurre gli sforzi e i costi di implementazione.
Foto_Teaser_SE-PR_PAD20_FoodTech-Award-2023_720x405-bg_hybris_teaser.png

Baumer Bubble Sensor PAD20 wins International FoodTec Award 2024

The unique PAD20 bubble sensor for air and gas bubble detection receives another innovation award. After winning the Dairy Technology Award 2021, the analysis sensor now convinced the expert jury granting the International FoodTec Award 2024 of the German Agricultural Society (DLG). What's so special about the PAD20? It is capable of detecting even tiniest gas bubbles in liquids, thus maximizing resource efficiency, food safety and overall equipment effectiveness.
In alto