Around 2000 skilled people commute daily from Eastern Switzerland to their employers in Zurich. That's why Baumer as part of the ProOst initiative is joining this year's Speed Dating for co-working in Frauenfeld!
En lançant la nouvelle génération de capteurs de pression hygiéniques de la série PP20H, Baumer complète sa gamme de produits et propose une solution, également à un prix intéressant, pour les applications hygiéniques exigeantes.
The hygienic pressure sensor PP20H was voted third place in the “Products of the year 2019” in the sensor category by the readers of the professional journal Elektronik. The pressure sensor PP20H with condensate-proof silicon measuring cell in IP69K-rated stainless steel housing meets the requirements of demanding hygienic applications.
With FLEX-3A, OTTO Vision Technology GmbH offers a high-end 3D scanner with a measuring range from 20 mm to 200 mm for non-contact 3D detection and geometry inspection of complex objects. Find out in our application report which is the role played by two cameras of the CX series with 12 megapixel and USB 3.0 interface.
The new DSRK strain probe from Baumer is setting new standards in tie bar strain measurement. Retaining the excellent measuring performance of its predecessor...
When it comes to tough outdoor use, many sensors reach their limits. Inclination sensors by sensor expert Baumer stand for maximum reliability and durability even in a harsh environment.
With their FlexFlow family of flow and temperature sensors, Baumer has expanded their process sensor portfolio. Based on the calorimetric measurement principle, the FlexFlow family...
With the new generation of universal temperature transmitters, FlexTop 2212 and 2222, Baumer is expanding its proven range of products. With integrated micro-USB port, automated cable compensation and ...
With the new PP20R family of pressure sensors, Baumer is expanding its portfolio to offer an attractively priced solution for demanding applications within the rail industry.
The Baumer LX VisualApplets cameras with integrated image preprocessing were honored with the highest award at this year‘s „Vision Systems Design Innovators Awards Program“.
What is the most efficient way to acquire rotation angles? It’s the Baumer magnetic absolute encoder series EAM580/360. Their precision is unrivalled; no product of another brand can compete in terms of robustness and longevity at this high level...
A new system allows for combine harvesters to maximize throughput without risking overload and blockages. Centrepiece of this innovative system is the forward-looking radar system by Baumer. The new Advanced Feedrate Control system for Case IH Axial-Flow combines now has been awarded a Silver Medal in the DLG Innovation Awards.