Quality meets economy – with the new product families U500 and UR18 Baumer sets the highest standards in ultrasonic sensor technology. The sensors for distance measurement and object detection are characterized by...
Aggressive media such as vapors or cleaning agents are at times a challenge for standard ultrasonic sensors. The sensor face, called a transducer, can be worn by these media and...
The possibility of bidirectional communication using the standardized IO-Link interface is the basis for new functions and services in the IIoT era. In addition to the primary function, such as a switching signal, additional secondary data provides valuable information about the production process. Access to the additional information allows the overall effectiveness of the system to be optimized and enables preventative maintenance.
Baumer has been selected as a recipient of a John Deere supplier innovation award for 2015. The award is presented to a select group of suppliers who have demonstrated innovation...
Inductive marine sensors by Baumer were specifically developed for use in harsh environments. In order to minimize the planning work involved in the development phase for onshore and offshore system manufacturers...
Progressive digitization and the trend towards individualized products also require solutions that are flexible and as automated as possible, even in the part inspection area.
The new high performance OM70 laser point and laser line distance sensors from Baumer combine high-precision measurement technology and easy handling in the automation industry.
Laser distance sensors enable high-precision distance and position measurement with a resolution of less than one micrometer. In practice, however, there are interference effects that can reduce the repeatability of optical distance measurements.
The O200 photoelectric miniature sensors from Baumer with IO-Link interface are the ideal solution for the detection demanding objects in confined spaces. With their unique ambient light immunity and their precise, reproducible and color-independent switching distances, the comprehensive portfolio offers absolute reliability even under difficult conditions.
Baumer Group has earned recognition as a Partner-level supplier in the John Deere Achieving Excellence Program. The Partner-level status is Deere & Company’s highest supplier rating.
Where do manufacturers in machinery and plant engineering get the best optical sensors, level switches and rotary encoders from? Answer: from Baumer. Customers know well that at Baumer they always get some extra performance on top as special support in tricky measuring tasks.
With the new PP20R family of pressure sensors, Baumer is expanding its portfolio to offer an attractively priced solution for demanding applications within the rail industry.
Inductive sensors very often form the basis for the reliable control of machines and systems.
In applications where non-ferrous metals such as aluminum need to be detected at the same working distance as steel, Factor 1 inductive sensors are a perfect fit. Baumer offers a unique selection of such sensors in switching and measuring versions.
When it comes to tough outdoor use, many sensors reach their limits. Inclination sensors by sensor expert Baumer stand for maximum reliability and durability even in a harsh environment.
Hyperloop, the project brought into being by Elon Musk, aims at revolutionizing mobility. Similar to the principle of pneumatic tube transport, people or goods travel without resistance and...
Quite many sensors meet their limits when it comes to measuring angles in harsh outdoor conditions. Inclination sensors in robust industrial design by sensor expert Baumer ensure reliable measurements...
Detecting objects with gaps or holes still constitutes a challenge for optical sensors in factory automation. With its new optical O300 miniature sensors with linear beam...
The Baumer optoelectronic sensors O200 are the first miniature sensors on the market to offer 3D CAD data with integrated beam path. This saves valuable time in the engineering process, which previously was quite an effort when integrating the beam path from data sheets.
Baumer has added a new model to its range of CombiLyz conductivity meters. In addition to the compact AFI4, the AFI5 version with remote sensor is now also available.
The new distance measuring inductive sensors AlphaProx with IO-Link interface from Baumer offer more than precise measurement technology. In addition to micrometer-precise distance values, two switching points...
To count, measure, detect – the tasks of Baumer sensors in machinery and installations are very clear. But there is much more to the small power packs. Many Baumer sensors feature IO-Link, a fast communication interface that besides measured values transmits a great bunch of additional information...
Get immersed in the fascinating world of sensor technology - following this motto in their last winter semester, students from different universities took the chance to get to know Baumer and the latest sensor technology.
Shorter and shorter product life cycles, wider product portfolios, increasing customer demands for individualization – these are the challenges facing manufacturing companies today.