Photoelectric sensors
Volumetric flow measurement
Software
Industrial cameras / image processing
Industrial cameras
Industrial cameras
Rotary encoders / angle measurement
Industrial cameras / image processing
Absolute HeavyDuty encoders
Ultrasonic distance measurement
Ultrasonic object detection
LX series (VLXT.I cameras)
Rotary encoders / angle measurement
LX series (VLXT cameras)
Incremental HeavyDuty encoders
Ultrasonic object detection / distance measurement
Object detection
Inductive proximity switches
Software
Industrial cameras / image processing
CX series (VCX.I cameras)
LX series (VLXT.FO cameras)
Industrial cameras
CX series (VCX.I cameras)
CX series (VCX.I.XT cameras)
CX series (VCX.I.PTP cameras)
Sensor accessories
Software
LX series (LXC cameras)
Easy sensor connection
Bearingless encoders
Reading 1D/2D codes
CX series (VCXG.SWIR.XC cameras)
Bearingless encoders for HeavyDuty applications
Counting quantities and events
LX series (LXG cameras)
The new sensor class for positioning and inspection tasks
Industrial cameras / image processing
LX series (VLXT.I.JP cameras)
Incremental HeavyDuty encoders
Incremental HeavyDuty encoders
Industrial cameras / image processing
Optical distance measurement
With measuring arm and wheel
Gigabit Ethernet, 2 Megapixel, Monochrome
Gigabit Ethernet, 2 Megapixel, Color
Dual GigE, 2 Megapixel, Monochrome
Dual GigE, 2 Megapixel, Color
Camera Link®, 2 Megapixel, Monochrome
Camera Link, 2 Megapixel, Color
Blind hollow shaft ø8 to ø14 mm
Sonic beam deflector series 20
Hygienic flow sensor
Flow sensor for industrial applications
Competitive pressure sensor for railway applications
Fully welded pressure sensor with hygienic connection
Miniaturized strain sensor for harsh industrial applications
Detection of air and gas bubbles for industrial applications
Hygienic compact RTD temperature sensor
The new O200 sensors from Baumer considerably raise the performance bar for optical miniature sensors. Economical in operation and featuring an impressive function variety in a standardized miniature housing...
Five new models with a 10 GigE Vision compliant interface for use with optical cables expand the Baumer LX series. The cameras are ideal for applications requiring a high bandwidth of 1.1 GB/s over long distances. In accordance with the SFP+ module used, long-distance solutions can be achieved up to 10 kilometers – without the need for media converters.
Safety through 100% quality control and product tracking
The Baumer CX.I cameras with their outstanding performance convinced the expert panel and participants of the online poll on the inspect award 2019 and were awarded 1st prize in the Vision category.
To count, measure, detect – the tasks of Baumer sensors in machinery and installations are very clear. But there is much more to the small power packs. Many Baumer sensors feature IO-Link, a fast communication interface that besides measured values transmits a great bunch of additional information...
We are talking with Lina De Windt today. She studies electrical engineering at ETH in Zurich and is an electrical engineer on the Swissloop team. In the interview, she tells us how she overcomes challenges in the testing phase with her team, how important team spirit is for this, and how successes are celebrated.
The CX.I cameras’ outstanding performance and optimized combination of mechanical and electrical capabilities have convinced the expert jury of the inspect award 2019 as well as the readers of the inspect and messtec drives Automation magazines and for this, they were awarded 1st prize in the vision category.
Thanks to four power outputs which can be triggered individually, the CX.I and LXT cameras allow for quick, easy and cost-efficient 3D surface inspections and identify even slightest non-compliance in structure and shape. Read our technical article on shape from shading and find out how it works.
With its O200 photoelectric miniature sensors, Baumer offers a new dimension in terms of reliability, speed and range for confined machine installation spaces. Thanks to their increased functional reserves, the O200 diffuse sensors with background suppression are the only ones with up to 120 mm sensing distance even on darkest and shiny objects such as mobile phone housings.