The new DSRK strain probe from Baumer is setting new standards in tie bar strain measurement. Retaining the excellent measuring performance of its predecessor...
Inductive sensors very often form the basis for the reliable control of machines and systems.
In applications where non-ferrous metals such as aluminum need to be detected at the same working distance as steel, Factor 1 inductive sensors are a perfect fit. Baumer offers a unique selection of such sensors in switching and measuring versions.
The new O300 miniature laser sensors with IO-Link by Baumer are the specialists for the reliable detection of very small objects and gaps. Thanks to a laser beam which focuses to within 0.1 mm and...
Quite many sensors meet their limits when it comes to measuring angles in harsh outdoor conditions. Inclination sensors in robust industrial design by sensor expert Baumer ensure reliable measurements...
The O200 photoelectric miniature sensors from Baumer with IO-Link interface are the ideal solution for the detection demanding objects in confined spaces. With their unique ambient light immunity and their precise, reproducible and color-independent switching distances, the comprehensive portfolio offers absolute reliability even under difficult conditions.
Sensor expert Baumer is further expanding their portfolio of cable transducers being the easiest, most reliable and cost-efficient way to measure linear motion within a path from 0.5 to 50 m.
With FLEX-3A, OTTO Vision Technology GmbH offers a high-end 3D scanner with a measuring range from 20 mm to 200 mm for non-contact 3D detection and geometry inspection of complex objects. Find out in our application report which is the role played by two cameras of the CX series with 12 megapixel and USB 3.0 interface.
With its O200 photoelectric miniature sensors, Baumer offers a new dimension in terms of reliability, speed and range for confined machine installation spaces. Thanks to their increased functional reserves, the O200 diffuse sensors with background suppression are the only ones with up to 120 mm sensing distance even on darkest and shiny objects such as mobile phone housings.
In machine tool spindles, miniature grippers, or robotics, space runs out in a hurry. Every integrator knows the pain of trying to get cable runs to work in the system, without compromising...
Demanding applications in machine and plant construction, for example in handling and assembly, graphic and packaging machines, require high precision in real-time with minimal cycle time and jitter.
Quality meets economy – with the new product families U500 and UR18 Baumer sets the highest standards in ultrasonic sensor technology. The sensors for distance measurement and object detection are characterized by...
The new distance measuring inductive sensors AlphaProx with IO-Link interface from Baumer offer more than precise measurement technology. In addition to micrometer-precise distance values, two switching points...
Detecting objects with gaps or holes still constitutes a challenge for optical sensors in factory automation. With its new optical O300 miniature sensors with linear beam...
Typically high shaft loads and situation-induced axial impact or overloads in shaft copying systems present a real challenge to encoders.
New, non-contact and fully encapsulated EB360 has been particularly designed for demanding tasks and is wear-free even in harsh environments.
With the new models from the AlphaProx family, Baumer has once more confirmed its position as one of the leading manufacturers in the field of measuring inductive sensors.
With the new AlphaProx IR12 and IR18 High Sensitivity sensors, Baumer is offering a true worldwide innovation: the first teachable standard inductive sensors for measuring tiny changes in position.
In many respects the requirements in the elevator industry are extremely high: maximum transportation comfort, minimal costs and zero defect tolerance during operation in the harshest environments.
Inductive marine sensors by Baumer were specifically developed for use in harsh environments. In order to minimize the planning work involved in the development phase for onshore and offshore system manufacturers...
Whether in industrial environments or in rough outdoor use – increasing of efficiency, reliability and durability are of primary importance.
Baumer offers the first CMOS cameras with an exposure time down to 1 µs in the mainstream segment of digital industrial cameras. The CX models including the second generation...
Baumer PosCon HM is a unique, compact measuring unit for the intelligent height measurement of objects with 5 key figures.
The measurement of object height is an important aspect in quality control applications. With the PosCon HM light-section sensor, Baumer offers a unique, compact measuring device for this kind of tasks.
Encoder expert Baumer has further expanded their HeavyDuty encoder portfolio. Newcomer POG 86E concentrates on the essential: pure function in corrosion-proof aluminium housing.