Inductive sensors very often form the basis for the reliable control of machines and systems.
In applications where non-ferrous metals such as aluminum need to be detected at the same working distance as steel, Factor 1 inductive sensors are a perfect fit. Baumer offers a unique selection of such sensors in switching and measuring versions.
Aggressive media such as vapors or cleaning agents are at times a challenge for standard ultrasonic sensors. The sensor face, called a transducer, can be worn by these media and...
The hygienic pressure sensor PP20H was voted third place in the “Products of the year 2019” in the sensor category by the readers of the professional journal Elektronik. The pressure sensor PP20H with condensate-proof silicon measuring cell in IP69K-rated stainless steel housing meets the requirements of demanding hygienic applications.
En lançant la nouvelle génération de capteurs de pression hygiéniques de la série PP20H, Baumer complète sa gamme de produits et propose une solution, également à un prix intéressant, pour les applications hygiéniques exigeantes.
With FLEX-3A, OTTO Vision Technology GmbH offers a high-end 3D scanner with a measuring range from 20 mm to 200 mm for non-contact 3D detection and geometry inspection of complex objects. Find out in our application report which is the role played by two cameras of the CX series with 12 megapixel and USB 3.0 interface.
The new DSRK strain probe from Baumer is setting new standards in tie bar strain measurement. Retaining the excellent measuring performance of its predecessor...
Baumer has added a new model to its range of CombiLyz conductivity meters. In addition to the compact AFI4, the AFI5 version with remote sensor is now also available.
With their FlexFlow family of flow and temperature sensors, Baumer has expanded their process sensor portfolio. Based on the calorimetric measurement principle, the FlexFlow family...
Sensor expert Baumer is further expanding their portfolio of cable transducers being the easiest, most reliable and cost-efficient way to measure linear motion within a path from 0.5 to 50 m.
Matching the begin of springtime, the new office building has been released from the scaffolding and presents itself with a real wow-effect. The quick progress is now obvious – with the sun protection having been installed and...
With the HMG10P / PMG10P series, Baumer raises the bar for HeavyDuty encoder technology. The encoders enable convenient configuration by any input device via WLAN adapter for individual configuration...
The new O300 miniature laser sensors with IO-Link by Baumer are the specialists for the reliable detection of very small objects and gaps. Thanks to a laser beam which focuses to within 0.1 mm and...
With the new O300 and O500 sensors in hygienic and washdown design, Baumer offers maximum reliability, comfort and minimum operating costs.
The new distance measuring inductive sensors AlphaProx with IO-Link interface from Baumer offer more than precise measurement technology. In addition to micrometer-precise distance values, two switching points...
To count, measure, detect – the tasks of Baumer sensors in machinery and installations are very clear. But there is much more to the small power packs. Many Baumer sensors feature IO-Link, a fast communication interface that besides measured values transmits a great bunch of additional information...
Measuring edge positions, object or column widths are important tasks in the part inspection process.
Demanding applications in machine and plant construction, for example in handling and assembly, graphic and packaging machines, require high precision in real-time with minimal cycle time and jitter.
A healthy mind in a healthy body
Five new models with a 10 GigE Vision compliant interface for use with optical cables expand the Baumer LX series. The cameras are ideal for applications requiring a high bandwidth of 1.1 GB/s over long distances. In accordance with the SFP+ module used, long-distance solutions can be achieved up to 10 kilometers – without the need for media converters.
In mining, there is a high responsibility for the performance and availability of machines as well as the product quality to be successful. Continuous operation, harsh environments, and remote locations also present extreme challenges. In this webinar recording you will learn how to meet these challenges with the help of Baumer sensors & HÜBNER BERLIN encoders.
This week, first concrete pillars for the future production building were erected and anchored in the soil. The precast concrete elements with up to 18m in height pave the way for the next step in the construction work...
The Baumer incremental encoder series OptoPulse® EIL580 presents a new family member with further enhanced protection against inductive shaft currents.
Typically high shaft loads and situation-induced axial impact or overloads in shaft copying systems present a real challenge to encoders.
Detecting objects with gaps or holes still constitutes a challenge for optical sensors in factory automation. With its new optical O300 miniature sensors with linear beam...
The O200 photoelectric miniature sensors from Baumer with IO-Link interface are the ideal solution for the detection demanding objects in confined spaces. With their unique ambient light immunity and their precise, reproducible and color-independent switching distances, the comprehensive portfolio offers absolute reliability even under difficult conditions.
The possibility of bidirectional communication using the standardized IO-Link interface is the basis for new functions and services in the IIoT era. In addition to the primary function, such as a switching signal, additional secondary data provides valuable information about the production process. Access to the additional information allows the overall effectiveness of the system to be optimized and enables preventative maintenance.
The Baumer optoelectronic sensors O200 are the first miniature sensors on the market to offer 3D CAD data with integrated beam path. This saves valuable time in the engineering process, which previously was quite an effort when integrating the beam path from data sheets.