Easy sensor connection
Use analog sensors and actuators efficiently in the IO-Link network
Efficiently integrate classic switching signals into IO-Link networks
Ultrasonic object detection / distance measurement
Inductive distance sensors
Exploit the full IO-Link potential
Sensor accessories
Force sensors / strain sensors
Accessories object / distance / 2D/3D sensors
Level sensors
Process sensors
Photoelectric sensors
Conductivity measurement
Photoelectric sensors
Force measurement
Process sensors
Bearingless encoders for industrial applications
Ultrasonic distance measurement
Level sensors
Miniature laser distance sensors
Object detection
Ultrasonic object detection
Temperature measurement
Flow measurement
Temperature measurement
Distance measurement
Object detection
Ultrasonic distance measurement
Object detection
Ultrasonic object detection
Photoelectric sensors
Process sensors
Distance measurement
Pressure measurement
Pressure measurement
Level sensors
Distance measurement
Pressure measurement
The smartest way to use IO-Link devices
Distance sensors
Distance sensors
Distance sensors
Distance sensors
Distance sensors
Distance sensors
Distance sensors
Distance sensors
Distance sensors
Distance sensors
Distance sensors
Distance sensors
Diffuse sensors with background suppression - washdown
SmartReflect Light barriers - washdown
SmartReflect Light barriers - transparent detection
SmartReflect Light barriers - transparent detection
SmartReflect Light barriers - transparent detection
SmartReflect Light barriers - transparent detection
SmartReflect Light barriers - standard
Diffuse sensors with background suppression - hygiene
SmartReflect Light barriers - transparent detection
SmartReflect Light barriers - transparent detection
SmartReflect Light barriers - standard
SmartReflect Light barriers - hygiene
SmartReflect Light barriers - hygiene
SmartReflect Light barriers - hygiene
Diffuse sensors with background suppression - hygiene
SmartReflect Light barriers - transparent detection
SmartReflect Light barriers - transparent detection
SmartReflect Light barriers - standard
SmartReflect Light barriers - hygiene
SmartReflect Light barriers - hygiene
SmartReflect Light barriers - hygiene
Diffuse contrast sensors
Diffuse contrast sensors - standard
Diffuse contrast sensors - standard
Retro-reflective sensors - for longer ranges
Retro-reflective sensors - for longer ranges
Retro-reflective sensors - standard
Retro-reflective sensors - standard
Retro-reflective sensors - standard
Retro-reflective sensors - standard
Retro-reflective sensors - for longer ranges
Retro-reflective sensors - for longer ranges
Retro-reflective sensors - for longer ranges
Baumer is pleased to announce the immediate availability of LBFH and LBFI level switches with IO-Link and ATEX approval. The IO-Link interface allows the user to automate...
The new distance measuring inductive sensors AlphaProx with IO-Link interface from Baumer offer more than precise measurement technology. In addition to micrometer-precise distance values, two switching points...
To count, measure, detect – the tasks of Baumer sensors in machinery and installations are very clear. But there is much more to the small power packs. Many Baumer sensors feature IO-Link, a fast communication interface that besides measured values transmits a great bunch of additional information...
For quick and easy access to IO-Link technology: the most important terms in brief and clearly explained.
Quality meets economy – with the new product families U500 and UR18 Baumer sets the highest standards in ultrasonic sensor technology. The sensors for distance measurement and object detection are characterized by...
The smartest way to use IO-Link devices
The possibility of bidirectional communication using the standardized IO-Link interface is the basis for new functions and services in the IIoT era. In addition to the primary function, such as a switching signal, additional secondary data provides valuable information about the production process. Access to the additional information allows the overall effectiveness of the system to be optimized and enables preventative maintenance.
With the new O300 and O500 sensors in hygienic and washdown design, Baumer offers maximum reliability, comfort and minimum operating costs.
The new O300 miniature laser sensors with IO-Link by Baumer are the specialists for the reliable detection of very small objects and gaps. Thanks to a laser beam which focuses to within 0.1 mm and...
Detecting objects with gaps or holes still constitutes a challenge for optical sensors in factory automation. With its new optical O300 miniature sensors with linear beam...
The O300 and O500 SmartReflect Transparent sensors set new standards in the detection of transparent objects. The light barrier without a reflector is the only sensor in its class ...
With their FlexFlow family of flow and temperature sensors, Baumer has expanded their process sensor portfolio. Based on the calorimetric measurement principle, the FlexFlow family...
Grippers & automatic tool changers
The O200 photoelectric miniature sensors from Baumer with IO-Link interface are the ideal solution for the detection demanding objects in confined spaces. With their unique ambient light immunity and their precise, reproducible and color-independent switching distances, the comprehensive portfolio offers absolute reliability even under difficult conditions.
En lançant la nouvelle génération de capteurs de pression hygiéniques de la série PP20H, Baumer complète sa gamme de produits et propose une solution, également à un prix intéressant, pour les applications hygiéniques exigeantes.
The hygienic pressure sensor PP20H was voted third place in the “Products of the year 2019” in the sensor category by the readers of the professional journal Elektronik. The pressure sensor PP20H with condensate-proof silicon measuring cell in IP69K-rated stainless steel housing meets the requirements of demanding hygienic applications.